This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1314R10: CAN I reflash without flashing the ccfg area?

Part Number: CC1314R10


Tool/software:

If i flash using jtag from CCS I get both code and ccfg.

If I reflash with a subsequent image, that has identical CCFG parameters, can I ommit flashing the CCFG, or is there something that prevents this?

I understand the image start of vector adresses is stored in ccfg, but not the start address itself, so if that is not

modified with a firmware upgrade that should work ???

Bulk erase should of course be avoided, since that erases CCFG as well, right??

Is there a serial programmer that can be customer installed and used to flash CC1314 ( via its serial porrt)?

Gullik

  • Hi Gullik,

    yes, you can use the ROM Bootloader to write a new image using UART.
    The procedure is explained here: https://www.ti.com/lit/swra466 and you'll also find a download link for an example.

    Kind regards,
    Theo

  • Thanks Theo,

    My understanding is then as follows....

    1) produce binary file from the "flash" section of the compiled image.

       (the CCFG part can be discarded if I did not change anything with syscfg )

    2) programming each flash sector by erasing / programming (similar to existing tools)

      using only the "flash" section.

    3) computing checksum to verify programming

    This would boot properly, IF the CCFG paramerters were not changed for this version / firmware update.

    Regards,

    Gullik