Other Parts Discussed in Thread: CC1352R, , CC1354P10, SYSCONFIG
Tool/software:
We are using a CC1354R10 on a CC1352R Launchpad.
I'm looking for the OneLib.a and StackWrapper.a files for the CC1354R10.
I only see below in the SDK libraries.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, are the files for the CC1354R10 not located in ble5stack_flash?
Also is there a reason why the cc13x2r1 files being used for the CC1354R10 series?
Hello Scot,
I was mistaken, I apologize! We're looking into this and will provide an answer by tomorrow (3/20).
Best Regards,
Tarek
Hello Scot,
Sorry for the delay! Upon checking with the team, I was informed that your team will be switching to the CC1354R10RGZ. So we would recommend using the CC1354P10_1 Folder.
Best Regards,
Tarek
Just to check, when you say I must use it, the problem is that compiler error says the folder should be named cc26x2. So I should make a copy of the CC1354P10_1 folder and rename it to that?
We are taking any BLE project for the CC1354P10, migrating in Sysconfig it to the CC1354R10 on a CC1352R Launchpad. Then we fix an issue with a missing rf_config.js files which causes sysconfig to not work. Then when we compile it says the cc26x2 folder which contains OneLib and StackWrapper is missing.
Hello Scot,
You're correct! Renaming could work. Another way of doing this, is to edit the Include Options search path and adding the missing folder. To do this, right click on the project and select properties. Then, go to Tools -> Arm Compiler -> Include Options. I hope this helps!
Please don't hesitate to let me know if you have any more questions.
Best Regards,
Tarek