Part Number: CC1312PSIP
Other Parts Discussed in Thread: TEST2
Tool/software:
Hi,
During our testing, we found that the TX current varies from batch to batch, which is causing issues with our automated testing during production.
Are these variations considered normal? I’m asking because the differences seem quite significant to me.
We also encountered another issue with the RX current. During testing, we found that three components were drawing around 25mA—double the expected value of approximately 12mA. After replacing those components, the current returned to normal, and everything functioned correctly.
You can see the results below. I’ve also attached a PDF file that includes a histogram for reference.
| 915 MHz | Laser Mark on SIP | |||||
| Min | Max | Average | Histogram | Data | ||
| Test1 | 45.2 | 50.1 | 47.4 | V | 17.12.2024 | 3CW1667 |
| Test2 | 47.4 | 50.2 | 47.4 | V | 23.01.2025 | 4AW2427 |
| Test3 | 46.7 | 63.9 | 60.7 | V | 10.02.2025 | 4BW2137 |
| 868 MHz | ||||||
| Min | Max | Average | Histogram | Data | ||
| Test1 | X | X | X | X | X | |
| Test2 | 38.0 | 43.9 | 40.1 | V | 23.01.2025 | 4AW2427 |
| Test3 | 45.3 | 50.9 | 47.4 | V | 11.02.2025 | 4BW2137 |
| Rx Current | Normal | 12.5mA | Fail/test | fail[%] | ||
| Fail | 25mA | 5/1200 | 0.42 | |||
E2E to TI Tx Rx Current Results.pdf
Thanks,
Shamai Yossi