This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: Can CCxxxx radio MCUs be programmed to function as a baseband chip (with an external mixer) ?

Part Number: CC1312R

Tool/software:

Colleagues,

Can CCxxxx radio MCUs be programmed to function as a baseband chip with an external mixer?  Is there a way to bypass or CCxxxx 's own mixer?

I’m looking for ICs which would help me build an HF radio link. My bands of interest are 14 MHz and 28 MHz amateur bands. I like the CCxxxx devices, because they have a lot of modulation options.  It would be neat if I could adapt them to HF bands by adding an external mixer.

Best regards,
- Nick