Tool/software:
I'm porting a design from SDK 6.10.0.29 to 8.30.1.01. I've run into a problem with the ADCBuf driver.
I'm using it in single shot mode to grab 400 samples at 10 kHz once every 20 seconds or so. This worked great in the SDK 6.10 world, but now the call to ADCBuf_convert fails with a -1 return code after one or two calls.
To make this easier to demonstrate, I've altered the adcbufcontinuous example to show the same behavior.
To demonstrate, simply load the adcbufcontinuous example, and replace the code in adcBufContinuousSampling.c with the code below.
You will note that for a few cycles the ADCBuf_convert call at line 168 will work, but it will eventually trap at line 171. I can discern no reason why this should happen. Ideas?
/*
* Copyright (c) 2015-2024, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following conditions
* are met:
*
* * Redistributions of source code must retain the above copyright
* notice, this list of conditions and the following disclaimer.
*
* * Redistributions in binary form must reproduce the above copyright
* notice, this list of conditions and the following disclaimer in the
* documentation and/or other materials provided with the distribution.
*
* * Neither the name of Texas Instruments Incorporated nor the names of
* its contributors may be used to endorse or promote products derived
* from this software without specific prior written permission.
*
* THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS"
* AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO,
* THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR
* PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR
* CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL,
* EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO,
* PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS;
* OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY,
* WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR
* OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE,
* EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
*/
/*
* ======== adcBufContinuousSampling.c ========
*/
#include <stdint.h>
#include <stdio.h>
#include <mqueue.h>
/* Driver Header files */
#include <ti/drivers/ADCBuf.h>
/* Display Header files */
#include <ti/display/Display.h>
/* Driver configuration */
#include "ti_drivers_config.h"
#define ADCSAMPLESIZE (400)
#define MAX_QUEUED_ADC_CONVERSIONS (4)
#define QUEUED_ADC_MESSAGE_SIZE (sizeof(uint32_t) * ADCSAMPLESIZE)
uint16_t sampleBufferOne[ADCSAMPLESIZE];
uint16_t sampleBufferTwo[ADCSAMPLESIZE];
uint32_t microVoltBuffer[ADCSAMPLESIZE];
uint32_t outputBuffer[ADCSAMPLESIZE];
uint32_t buffersCompletedCounter = 0;
/* Display Driver Handle */
Display_Handle displayHandle;
/* Used to pass ADC data between callback and main task */
static mqd_t queueReceive;
static mqd_t queueSend;
/*
* This function is called whenever an ADC buffer is full.
* The content of the buffer is then converted into human-readable format and
* sent to the main thread.
*/
void adcBufCallback(ADCBuf_Handle handle,
ADCBuf_Conversion *conversion,
void *completedADCBuffer,
uint32_t completedChannel,
int_fast16_t status)
{
/* Adjust raw ADC values and convert them to microvolts */
ADCBuf_adjustRawValues(handle, completedADCBuffer, ADCSAMPLESIZE, completedChannel);
ADCBuf_convertAdjustedToMicroVolts(handle, completedChannel, completedADCBuffer, microVoltBuffer, ADCSAMPLESIZE);
/* Send ADC data to main thread using message queue */
mq_send(queueSend, (char *)microVoltBuffer, QUEUED_ADC_MESSAGE_SIZE, 0);
}
/*
* ======== mainThread ========
*/
void *mainThread(void *arg0)
{
Display_Params displayParams;
ADCBuf_Handle adcBuf;
ADCBuf_Params adcBufParams;
ADCBuf_Conversion continuousConversion;
ADCBuf_Conversion Conversion;
struct mq_attr attr;
uint32_t average;
uint_fast16_t i = 0;
/* Create RTOS Queue */
attr.mq_flags = 0;
attr.mq_maxmsg = MAX_QUEUED_ADC_CONVERSIONS;
attr.mq_msgsize = QUEUED_ADC_MESSAGE_SIZE;
attr.mq_curmsgs = 0;
queueReceive = mq_open("ADCBuf", O_RDWR | O_CREAT, 0664, &attr);
queueSend = mq_open("ADCBuf", O_RDWR | O_CREAT | O_NONBLOCK, 0664, &attr);
if ((queueReceive == (mqd_t)-1) || (queueSend == (mqd_t)-1))
{
/* Failed to open message queue */
while (1) {}
}
/* Call driver init functions */
ADCBuf_init();
Display_init();
/* Configure & open Display driver */
Display_Params_init(&displayParams);
displayParams.lineClearMode = DISPLAY_CLEAR_BOTH;
displayHandle = Display_open(Display_Type_UART, &displayParams);
if (displayHandle == NULL)
{
Display_printf(displayHandle, 0, 0, "Error creating displayHandle\n");
while (1) {}
}
Display_printf(displayHandle, 0, 0, "Starting the ADCBufContinuous example");
// /* Set up an ADCBuf peripheral in ADCBuf_RECURRENCE_MODE_CONTINUOUS */
// ADCBuf_Params_init(&adcBufParams);
// adcBufParams.callbackFxn = adcBufCallback;
// adcBufParams.recurrenceMode = ADCBuf_RECURRENCE_MODE_CONTINUOUS;
// adcBufParams.returnMode = ADCBuf_RETURN_MODE_CALLBACK;
// adcBufParams.samplingFrequency = 1000;
// adcBuf = ADCBuf_open(CONFIG_ADCBUF_0, &adcBufParams);
// /* Configure the conversion struct */
// continuousConversion.arg = NULL;
// continuousConversion.adcChannel = CONFIG_ADCBUF_0_CHANNEL_0;
// continuousConversion.sampleBuffer = sampleBufferOne;
// continuousConversion.sampleBufferTwo = sampleBufferTwo;
// continuousConversion.samplesRequestedCount = ADCSAMPLESIZE;
while(1)
{
/* Set up an ADCBuf peripheral in ADCBuf_RECURRENCE_MODE_ONE_SHOT */
ADCBuf_Params_init(&adcBufParams);
adcBufParams.callbackFxn = NULL;
adcBufParams.recurrenceMode = ADCBuf_RECURRENCE_MODE_ONE_SHOT;
adcBufParams.returnMode = ADCBuf_RETURN_MODE_BLOCKING;
adcBufParams.samplingFrequency = 10000;
adcBuf = ADCBuf_open(CONFIG_ADCBUF_0, &adcBufParams);
/* Configure the conversion struct */
Conversion.arg = NULL;
Conversion.adcChannel = CONFIG_ADCBUF_0_CHANNEL_0;
Conversion.sampleBuffer = sampleBufferOne;
Conversion.sampleBufferTwo = NULL;
Conversion.samplesRequestedCount = ADCSAMPLESIZE;
if (adcBuf == NULL)
{
/* ADCBuf failed to open. */
while (1) {}
}
/* Start converting. */
if (ADCBuf_convert(adcBuf, &Conversion, 1) != ADCBuf_STATUS_SUCCESS)
{
/* Did not start conversion process correctly. */
while (1) {}
}
/* Adjust raw ADC values and convert them to microvolts */
ADCBuf_adjustRawValues(adcBuf, sampleBufferOne, ADCSAMPLESIZE, CONFIG_ADCBUF_0_CHANNEL_0);
ADCBuf_convertAdjustedToMicroVolts(adcBuf, CONFIG_ADCBUF_0_CHANNEL_0, sampleBufferOne, (uint32_t*)outputBuffer, ADCSAMPLESIZE);
ADCBuf_close(adcBuf);
}
/*
* Wait for the message queue to receive ADC data from the callback
* function. When data is received, calculate the average and print to UART
*/
while (1)
{
if (mq_receive(queueReceive, (char *)outputBuffer, QUEUED_ADC_MESSAGE_SIZE, NULL) == -1)
{
Display_printf(displayHandle, 0, 0, "Error receiving ADC message");
while (1) {}
}
Display_printf(displayHandle, 0, 0, "Buffer %u finished:", (unsigned int)buffersCompletedCounter++);
/* Calculate average ADC data value in uV */
average = 0;
for (i = 0; i < ADCSAMPLESIZE; i++)
{
average += outputBuffer[i];
}
average = average / ADCSAMPLESIZE;
/* Print average ADCBuf value */
Display_printf(displayHandle, 0, 0, " Average: %u uV", average);
}
}