Other Parts Discussed in Thread: CC1352P7, CCSTUDIO
Tool/software:
The LP-XDS110ET, Launchpad Connector P10, on which pin detects the Target's power?
The custom target board is powered externally.
"IcePick_C: Error connecting to the target: (Error -180 @ 0x0) The controller has detected a target power loss. The user must turn-on or connect the power supply for the target. (Emulation package 20.1.0.3372)"
My understanding is that
- Pin3 is a 5V source for the target
- Pin 5 is a 3.3V source for the target and the pin on which the current consumption is measured with Energy Trace.
- Pin 4 and 6 is not connected on the LP-XDS110ET PCB.
Remark:
On the LP-XDS110ET PCB the Launchpad Connector P10 is reversed: the pin1 on the connector is PIN19 on the PCB.