Other Parts Discussed in Thread: LP-CC1311P3, , SYSCONFIG, CC1312PSIP
Tool/software:
Hi experts,
Q1: Does the LP-EM-CC1312PSIP or LP-CC1311P3 support the following?
Q2: Also, are there any devices or EVMs that support the following?
Q3: Could you please tell me how to set the following RF settings based on the sample code in CCS? It's okay if you can't use Sysconfig.
- Frequency 365.075MHz and 365.325MHz
- Modulation method 4-level FSK
- Modulation speed 7200bps
Best regards,
O.H