Tool/software:
Hi Team,
When I enable "Force VDDR" and set the TX Power to 12.5 dBm (or lower) in the .syscfg GUI menu, it shows the following aleart.
"The selected TX Power requires Force VDDR in Device Configuration to be disabled, otherwise the output power may be wrong and the current draw too high."
Could you please clarify if the only issues with this setting are the deviation from the set output power and increased current consumption? Are there any other potential issues that we should be aware of?
The background for my inquiry is that our device needs to support an output power of 14 dBm, while also having the capability to reduce output power in certain situations (such as when operationg in different regsions).
Thanks,
Tetsu