Tool/software:
My customer met an issue during developing a program to interface with CC113L The read out from RXBYTES register(0x3B) is always 0. Would you please help check if there is anything missing from the configuration?
Parameters of the transmitter side:
- MANCHESTER encoding
- Data rate: 9.6kbps
- Bit width: 104us
- Modulation: FSK
- Carrier wave frequency: 433.92MHz ± 30kHz
- FSK deviation: 60kHz
CC113L SmartRF Studio configuration as below:

The exported register values as below:

The host MCU code as below:

The SPI communication between the host MCU and CC113L has been verified and fine, but CC113L did not receive data as expected. Please help review the settings, thanks.
Best regards,
Shuyang