Software: Smartrf Studio_7-2.28.0
Hardware: Smartrf EV0B CC1101
The connection between SmarrfEV0B and CC1101 has SPI wire, VCC and GND
Question:
Connect the CC1101 access software using Smartrf EV0B. One configuration is for receiving and the other is for sending. However, the test found that there was an RSSI signal in the Continue RX window of the receiver, but no data was received in the Packet RX window.The configuration parameters are as follows:
- What problem caused it?
- How to troubleshoot such problems.
- Are there any other parameters that need to be configured?
Please help review the settings, thanks.
Best regards,
HuangChaoyu