This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1101: RSSI Not changing when I transmit from my other device

Part Number: CC1101

Tool/software:

I am trying to detect a 433mhz signal from a tpms sensor.

I am setting the cc1101 to direct mode because I want to process all of the raw signals in software on my MCU.

I can see a ton of pulses coming via the gpo0 pin on the cc1101 to my MCU. I am sure most of it is noise, so I need to use the RSSI to detect when my signal is being sent.

I can see on my log output the RSSI value and it is always about 0xA5.

This doesn't change when I know I am sending a signal from the tpms sensor. I have another app running on my PC that shows the tpms sensor data so I know it is actually sending something.

The device is withint 12 inches of the cc1101 antenna.

Can I get RSSI in raw direct mode or do I have to set up some kind of packet settings on the cc1101?