This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1110-CC1111: Re: RF transceiver IC product suggestion for frequnecy bands

Part Number: CC1110-CC1111

Tool/software:

Hi,

Please suggest any transceiver ICs that supports frequency bands with less works in Tuning.

TX bands -  121.5 MHz, 243 MHz , 406 MHz

RX bands - 121.5 MHz, 243 MHz.

Transceiver IC should support digital interface like Serdes, UART, SPI etc.,

Thanks in advance.