Other Parts Discussed in Thread: SYSCONFIG,
Tool/software:
Hi,
We can have a specific configuration requirement to be implemented on CC1311. Please check and comment on the below configuration possibility in CC1311.
FEC: 1/2 rate convolutional coding
Preamble (4 bytes): AAAAAAAA
Sync Word (4 bytes): 91D391D3
Whitening : Enabled as in CC1110
Deviation: 3.707866 kHz
Channel spacing: 363372.8027
Manchester Encoding : Disabled
Modulation: 2-FSK
Center Frequency : 400.2 MHz and 450.1 MHz
IF Frequency : 158.203 kHz
Frequency Offset : 0
Thanks,
Theiv