Tool/software:
Dear TI Support Team,
I am developing with the following environment:
-
MCU: CC2651R3SIPA
-
SDK: simplelink_cc13xx_cc26xx_sdk_7_41_00_17
-
OS: TI RTOS
I would like to use an External LF Clock as the 32 kHz low-frequency clock source instead of XOSC_LF. However, despite changing the settings in the syscfg file, I am unable to make it work. Even when connecting the debugger and starting, an error is displayed.
I am attaching a screenshot of my syscfg file. Could you please advise if there are other settings that need to be configured? Also, if there are any registers or other software changes required to enable the external LF clock, I would appreciate your guidance.
Thank you very much for your support.

Best regards,
Hiroki Saitoh