This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1200: Is it possible to receive the output of CC1020 with CC1200?

Expert 2490 points
Part Number: CC1200
Other Parts Discussed in Thread: CC1020,

Tool/software:

Hi All,

・The output band of CC1020 is 426MHz.
・BPS (H, L) is controlled by entering H and L into DIO.
H=3.3ms, L=1.68ms

Is it possible to receive the output of CC1020 with CC1200?

Best Regards,

Ito

  • Hi,

    It should be possible to receive the output from CC1020 with CC1200.

    Please make sure the packet PHY configuration is exactly the same for the two devices (data rate, preamble, sync, data length, modulation type, frequency deviation etc).