Tool/software:
Hello,
I'm working with the CC1312R1F3RGZR chip and I need a documented specification for the maximum *continuous* current allowed through the internal ESD clamp diodes on GPIO pins (diodes to VDD and GND).
- The datasheet provides the voltage limits (–0.3 V to VDD + 0.3 V), implying clamping diodes exist.
- However, it does not specify the maximum continuous or peak clamp current allowed through those diodes.
Could you please clarify:
1. What is the **maximum continuous current** allowed through a clamp diode (e.g. during input overvoltage conditions with series resistor)?
2. Is 2 mA considered safe for long-term operation?
3. Is there any official document or application note that gives this information specifically for the CC13x2/CC26x2 family?
Thank you in advance.