Tool/software:
Hi,
I am configuring a CC1352R using the PHY ID 132. This ID gives me the following specifications:
Data Rate: 200 kbps
Channel 0 Feq: 902.4 MHz
# of Channels: 64
Channel Spacing: 400 kHz.
With them in mind, I have two questions:
- What is the 6 dB bandwidth of each channel using this PHY ID? I couldn't find this information in the documentation.
- Is it possible to change any configuration to increase the channel spacing and achieve a bandwidth greater than 500 kHz per channel? I am willing to sacrifice the number of channels, but I cannot change the data rate or the frequency of Channel 0.
Thanks