This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1311R3: Link between CC1125 and CC1311

Part Number: CC1311R3
Other Parts Discussed in Thread: CC1125

Tool/software:

My customer wants to use CC1311 to communicate to a gateway running on CC1125. The PHY settings on CC1125 is as below:

  • Frequency: 869.2125 MHz
  • Modulation: GFSK NRZ
  • Deviation: ±3kHz
  • Channel:12.5kHz
  • Bit rate: 4800 bits/s

And the modulation detail is as below:

Would you please help confirm if CC1311 can support this PHY? Thanks.

Best regards,

Shuyang Zhong