Part Number: CC2340R5
Tool/software:
When using the SmartRF CLI command line to send instructions, setting the typical PHY prompted the error message "Invalid typical PHY name".
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CC2340R5
Tool/software:
When using the SmartRF CLI command line to send instructions, setting the typical PHY prompted the error message "Invalid typical PHY name".
Hello Carson Chenn,
Referencing the help documentation, we should be able to use one of the commands below:
PHY OPERATIONS
--print-typical-phys
Print <Typical PHY name> for all typical PHYs available in the current
workspace.
--select-typical-phy "<Typical PHY name>"
Select the specified typical PHY. If successful, this becomes the current
PHY.
--print-custom-phys
Print <Custom PHY name> for all custom PHYs in the current workspace.
Nothing will be printed if there are no custom PHYs in the workspace.
--select-custom-phy "<Custom PHY name>"
Select the specified custom PHY. If successful, this becomes the current
PHY.
--create-custom-phy "<Custom PHY name>"
Create a new custom PHY, with the specified name, based on the current PHY.
If successful, this becomes the current PHY.
--remove-custom-phy "<Custom PHY name>"
Remove the specified custom PHY. If this is the current PHY, there will be
no current PHY after the operation.
Thanks,
Alex F