Hello all , i want to use the feature of MSP430FR5739 to collaborate with RF2500 so that there is fast data writing and very low power comnsumption of controller itself which can have a lot of benefits. For this i want to ask some basic questions.
1. How to connect the Fraunch Pad and RF2500 ? like powering up both by same source such as a solar panel or SEH kit available from TI and how should both be programmed from same source. i.e USB emulator within RF2500 kit. I can configure ADC, clocks and all so i think programming wouldnt be a problem . But i am confused with the Hardware connection as i am pretty new at this. Because what i can come up is .
RF2500's emulator will program MSP430FR5739--->MSP will sample-->MSP will send data to RF2500----> then it will send data wirelessly to RF2500 connected at PC.
So basically it is like i want to remove the MSP430 already connected to RF2500 target board kit and replace with FRAM.
Any help would be greatly appreciated like i dont know from where to begin. I know about MSP430FR5739 pretty good. But nothing about RF2500 and how to connect it.
Thnx