This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: RF Performance Degradation

Part Number: CC1310


Tool/software:

We have been using Qualcomm SAW filter (Part Number: B39871B3717U410)  which incorporates the TI CC1310 chipset.
Issue Summary:
The affected product was assembled and tested successfully in February 2021 and subsequently shipped to the customer.
However, the customer did not install or power on the unit for approximately 3 to 4 years. During this time, the unit was stored in both indoor and outdoor environments.
Recently Observed Behavior:
During installation, our team identified a significant issue with RF communication performance. After detailed troubleshooting, the following was observed:
Up to 80% degradation in RF communication range.
No issues found in firmware or digital circuitry.
The degradation was isolated to the RF path, specifically pointing to the SAW filter.
We would appreciate any relevant data, failure modes, or guidance you can share to support our analysis and preventive actions moving forward.
Product Summary:
Product: Individual Lamp Monitoring RF Unit
Chipset: TI CC1310
SAW Filter Part Number: B39871B3717U410
Assembly Date: February 2021
Storage Duration: ~4 years (Assembled and unpowered)
Used Cabinet: IP67
Storage Conditions: Indoor/outdoor (approx 50 degree Celsius)
  • Hi,

    Sorry to hear about this issue.

    Have you tried A/B testing?
    I'll check with the device experts if we have such data available for CC1310; at the same time, for the Qualcomm part, have you reached out to them about this issue?

    Thanks,
    Toby

  • Hi Toby,

    We did a initial test  before the degrade and after degrade in this case after degrade RSSI result is above -95dBm but the before degrade we got values -60 to  -70 dBm

  • Hi,

    Please can you clarify whether the RX performance is regained if you replace the SAW filter with a part that wasn't stored in the same conditions?

    As Toby mentioned, if you perform A/B testing with the device what are the observed results?

    Regards,
    Zack

  • Hi 

    As I said earlier,

    We did a test before the degrade and after degrade in this case after degrade RSSI result is above -95dBm but the before degrade we got values -60 to  -70 dBm

  • Hi,

    Yes but that does not answer the questions we asked to try and isolate the root cause. We cannot futher investigate the issue if the only information we have is that before storage the reported RSSI result was between -60 dBm to -70 dBm and after storage it is reported as above -95 dBm. More tests are required.

    If a degradation of the SAW filter performance is found to be the root cause, you will need to reach out to Qualcomm regarding that part.

    Regards,

    Zack