This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: Request for Guidance: Communication Between TI CC1310 and STM32WL55 (LoRa/Sigfox)

Part Number: CC1310

Tool/software:

Sir/Madam,

We are currently working on a wireless communication project involving two different platforms:

  • TI CC1310

  • STMicroelectronics STM32WL55

Our aim is to establish communication between these two platforms for range and signal performance testing. The STM32WL55 supports LoRa, FSK, GFSK, and OOK modulation schemes. The CC1310 supports FSK, GFSK, OOK, and can also be configured for Sigfox using RF core overrides, as previously documented on your wiki.

I came across this reference:

"LoRa chip is only available from Semtech. CC1310 supports SIGFOX which you can refer to 'processors.wiki.ti.com/.../Sigfox_CC1310_SDK_Demo_Users_Guide' and it can compete to LoRa."

Unfortunately, the above wiki link no longer opens We would appreciate if you could help us with:

  1. Access to the Sigfox CC1310 SDK Demo Guide or equivalent documentation.

  2. Updated software/firmware resources for enabling Sigfox mode on the CC1310 (Zone 1/3 support).

  3. Guidance on how to configure CC1310 and STM32WL55 to communicate using a common modulation scheme like FSK, for testing purposes.

  4. Recommended RF parameters for such interoperability (frequency, data rate, deviation, etc.).

I intend to test one module as a transmitter and the other as a receiver, to evaluate signal strength (RSSI), SNR, and range performance.

Thank you for your assistance. We look forward to your support.

Thank you,

Chinmay

  • Hi Chinmay,

    The engineer who supported this at the time (and will have the most useful input) is on leave, so we will have to reply to this next week when he is back in the office.

    Regards,

    Zack