This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: Enabling any of the load monitoring in syscfg breaks the build

Part Number: CC1312R
Other Parts Discussed in Thread: SYSBIOS

Tool/software:

linux ubuntu 24.04 

brand new install of Version: 12.8.1.00005

installed simplelink_cc13xx_cc26xx_sdk_8_30_01_01

new workspace

create  sensor_oad_onchip_secure project

build

run

runs

open rov 

lots of stuff missing 

open syscfg

click add on the Ti RTOS\Utils\Load option to add all the extra bits

save

build

this happens

remove the load section again

project builds

this is all stock, nothing altered in the project settings or syscfg except that additional load module