This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1312R: Partial receive mode race condition with SPI peripheral

Part Number: CC1312R
Other Parts Discussed in Thread: SYSCONFIG

Tool/software:

I am using the partial receive mode on the advanced Rx command on a CC1312. I'm receiving UAT packets, which don't include a length field nad need to have their type code and preamble investigated to know their expected length. They have a wide range of lengrhs, ranging from 34 to 552 bytes. Right now I am using the partial receive mode to receive these packets, so I set maxPktLen to 0, and then set the expected packet length in the rx callback after the N bytes received event is triggered. This works great until I enable my SPI interrupts, in which case I eventually get a full microcontroller crash after somewhere between a few minutes and a few hours (while subjecting the device to heavy packet load).

My best guess is that somewhere along the line, the SPI interrupt stomps on the RF event that would trigger a packet length write, and the RF core writes well beyond the end of the packet buffer and corrupts other memory.

I tried to address this by setting maxPktLen to 552 bytes, the max packet size I would ever expect (which my partial receive buffer is sized to handle), but then all of my partial receive packets seem to ignore my RF_cmdPropSetLen and always return with a length equal to my max packet size.

I've tried playing with interrupt priorities, by reducing the hardware and software interrupt priorities of the SPI peripheral compared to the RF peripheral in sysconfig, but this doesn't completely solve the problem. Currently the only way I can solve this problem reliably is to hardcode maxPktLen to 552 bytes, but if I do this I'm wasting a large amount of valuable airtime by ingesting 552 bytes for every 34 byte packet (there are a lot more 34 byte packets than 552 byte packets).

Do you have any tips for solving this problem? A snippet of my code is included below (C++).

```

#include "sub_ghz_radio.hh"

#include "hal.hh"
#include "macros.hh"
#include "pico.hh" // For LED blinks.
#include "uat_packet_decoder.hh"
#include "unit_conversions.hh" // for CeilBitsToBytes

extern "C" {
#include "ti/devices/cc13x2_cc26x2/driverlib/rf_prop_mailbox.h" // For status codes.
}

static const uint32_t kRxRestartTimeoutMs = 5000;

static const uint16_t kNumPartialDataEntries = SubGHzRadio::kRxPacketQueueLen;
static const uint16_t kPartialDataEntryHeaderSizeBytes = 12;
static const uint16_t kPartialDataEntryNumAppendedBytes = 6; // Appended Bytes determined by the settings below.
static const uint16_t kPartialDataEntryPayloadSizeBytes = SubGHzRadio::kRxPacketMaxLenBytes;
static const uint16_t kPartialDataEntryPayloadLenSzBytes = 2; // Length field size in bytes.

static const uint16_t kPacketHeaderSizeBytes = 1; // Equivalent to CeilBitsToBytes(RF_cmdPropRxAdv.hdrConf.numHdrBits);

static const uint16_t kPartialDataEntrySizeBytes = sizeof(rfc_dataEntryPartial_t) + kPartialDataEntryPayloadLenSzBytes +
kPacketHeaderSizeBytes + kPartialDataEntryPayloadSizeBytes +
kPartialDataEntryNumAppendedBytes;
static_assert(kPartialDataEntryHeaderSizeBytes % 4 == 0, "Partial Data Entry Header Size must be word aligned.");

static const RF_EventMask kRxEventMask =
RF_EventMdmSoft | RF_EventNDataWritten | (RF_EventRxEntryDone | RF_EventRxOk | RF_EventRxNOk) |
(RF_EventLastCmdDone | RF_EventCmdCancelled | RF_EventCmdAborted | RF_EventCmdStopped);

static volatile uint16_t current_packet_len_bytes = 0;

// Packet RX Configuration
// ------------------------------------------------------------------------------------------------------------------------
// | Partial Data Entry Header | Payload Length (lenSz Bytes) | Payload Bytes | Optional Appended Bytes
// ------------------------------------------------------------------------------------------------------------------------

// Optional appended bytes
// -------------------------------------------------------
// | CRC1 | CRC0 | RSSI | TS0 | TS1 | TS2 | TS3 | Status |
// -------------------------------------------------------
static uint8_t rx_data_entry_buf[kNumPartialDataEntries * kPartialDataEntrySizeBytes] __attribute__((aligned(4)));
static rfc_dataEntryPartial_t *partial_data_entry_ptrs[kNumPartialDataEntries] = {0};

// This is the entry that we are currently allowed to read from (not being used by the RF core).
static rfc_dataEntryPartial_t *current_read_entry;

static dataQueue_t rx_data_queue;
static bool rx_data_length_written = false;

inline void RollDataQueue() {
current_read_entry->status = DATA_ENTRY_PENDING;
current_read_entry = (rfc_dataEntryPartial_t *)(((rfc_dataEntryPartial_t *)current_read_entry)->pNextEntry);
rx_data_queue.pCurrEntry = (uint8_t *)current_read_entry;
}

// Technical Reference Manual Section 23.7.5.4: www.ti.com/.../swcu117i.pdf
void rf_cmd_callback(RF_Handle h, RF_CmdHandle ch, RF_EventMask e) {
// CONSOLE_INFO("SubGHzRadio", "RF command completed with handle %p, command handle %d, event mask %u", h, ch, e);

if (e & RF_EventMdmSoft) {
// Preamble detected. Get ready to figure out packet length!
rx_data_length_written = false;
}

if (e & RF_EventNDataWritten) {
if (!rx_data_length_written) {
// Only set the length once, after receiving the first two bytes of the packet.
rx_data_length_written = true;

// TODO: Set this value based on bytes received so far.
current_packet_len_bytes = 34;

rfc_CMD_PROP_SET_LEN_t RF_cmdPropSetLen = {.commandNo = CMD_PROP_SET_LEN,
.rxLen = (uint16_t)(current_packet_len_bytes)};
RF_runImmediateCmd(h, (uint32_t *)&RF_cmdPropSetLen);
}
}

if (e & RF_EventRxOk) {
subg_radio.HandlePacketRx((rfc_dataEntryPartial_t *)(current_read_entry));
}

if (e & (RF_EventLastCmdDone | RF_EventCmdAborted | RF_EventRxBufFull)) {
// subg_radio.HandlePacketRx((rfc_dataEntryPartial_t *)(rx_data_queue.pLastEntry));
RollDataQueue();
// rx_ended = true;
}
}

bool SubGHzRadio::Init() {
RF_Params rf_params;
RF_Params_init(&rf_params);

// Overriding settings from smartrf/smartrf_settings.c.
/* RF_cmdPropRxAdv - Advanced Rx command settings. */
RF_cmdPropRxAdv.pQueue = &rx_data_queue;
RF_cmdPropRxAdv.pOutput = (uint8_t *)&rx_statistics_;
RF_cmdPropRxAdv.rxConf = {
.bAutoFlushIgnored = 0, // If 1, automatically discard ignored packets from RX queue.
.bAutoFlushCrcErr = 0, // If 1, automatically discard packets with CRC error from RX queue.
// bIncludeHdr must be 1 to receive the first byte after sync in the data entry. For UAT this is the last byte
// of the full 36 bit sync word.
.bIncludeHdr =
1, // If 1, include the received header or length byte in the stored packet; otherwise discard it.
.bIncludeCrc = 0, // 2 bytes (if default CRC is used)
.bAppendRssi = 1, // 1 byte
.bAppendTimestamp = 1, // 4 bytes
.bAppendStatus = 1 // 1 Byte
};
// RF_cmdPropRxAdv.pktConf.bRepeatOk = 0; // Go back to sync search after receiving a packet correctly.
// RF_cmdPropRxAdv.pktConf.bRepeatNok = 0; // Go back to sync search after receiving a packet incorrectly.
// Sync on the most significant 32 bits of the 36 bit sync word. Save the last 4 bits of sync for discrimination
// between uplink and ADSB packets in the payload. RF_cmdPropRx.syncWord = RawUATADSBPacket::kSyncWordMS32;
RF_cmdPropRxAdv.syncWord0 = RawUATADSBPacket::kSyncWordMS32;
RF_cmdPropRxAdv.syncWord1 = RawUATUplinkPacket::kSyncWordMS32;

// This needs to be set to 0, or else the length can't be overridden dynamically.
// WARNING: Setting packet length via the RF command callback can get stomped by another interrupt context (e.g.
// SPI). This leads to the RF core writing infinitely into memory, causing a non-deterministic crash behavior. Make
// sure the software interrupt priority for the RF system is higher than the software interrupt priority for SPI (I
// set hardware interrupt priority higher too, but that doesn't seem to fix it on its own). Setting RF software
// interrupt priority 1 point higher than SPI interrupt priority seems to work well. Higher values for RF software
// interrupt priority lead to crashes. To sidestep this drama, just set the max expected packet length as maxPktLen
// and take the performance hit (more rx airtime wasted per packet received).
RF_cmdPropRxAdv.maxPktLen = 0; // 0 = unlimited / unknown length packet mode

// The last 4 bits of the Sync word are interpreted as the header, so the rest of the packet stays byte-aligned.
RF_cmdPropRxAdv.hdrConf = {.numHdrBits = 4, .lenPos = 0, .numLenBits = 0};

// No address field.
RF_cmdPropRxAdv.addrConf = {0};

/* RF_cmdPropRadioDivSetup - Radio setup command settings. */
RF_cmdPropRadioDivSetup.formatConf.nSwBits =
32; // Use a 32-bit sync word to allow the last 4 bits of the sync to be used for format discrimination.

// Set up the data queue.
for (uint16_t i = 0; i < kNumPartialDataEntries; i++) {
// Fill out the addresses first so that our pNextEntry assignment works in the next loop.
partial_data_entry_ptrs[i] = (rfc_dataEntryPartial_t *)&rx_data_entry_buf[i * kPartialDataEntrySizeBytes];
}

for (uint16_t i = 0; i < kNumPartialDataEntries; i++) {
rfc_dataEntryPartial_t *entry = partial_data_entry_ptrs[i];
entry->length = sizeof(rfc_dataEntryPartial_t::pktStatus) + sizeof(rfc_dataEntryPartial_t::nextIndex) +
kPacketHeaderSizeBytes + kPartialDataEntryPayloadLenSzBytes +
kPartialDataEntryPayloadSizeBytes + kPartialDataEntryNumAppendedBytes;
entry->config.irqIntv = 0; // Set interrupt interval. We only need 1 byte after the header, increase to reduce
// interrupt frequency. 0=16
entry->config.type = DATA_ENTRY_TYPE_PARTIAL;
entry->config.lenSz = kPartialDataEntryPayloadLenSzBytes;
entry->status = DATA_ENTRY_PENDING;
entry->pNextEntry = (uint8_t *)partial_data_entry_ptrs[(i + 1) % kNumPartialDataEntries]; // Circular queue.

// Sentinel values for debuging.
memset(&(entry->rxData) + kPartialDataEntryPayloadLenSzBytes, 0xAA + i,
kPartialDataEntryPayloadSizeBytes + kPartialDataEntryNumAppendedBytes);
}
rx_data_queue.pCurrEntry = (uint8_t *)partial_data_entry_ptrs[0];
rx_data_queue.pLastEntry = nullptr;

current_read_entry = (rfc_dataEntryPartial_t *)(rx_data_queue.pCurrEntry);

rf_handle_ = RF_open(&rf_object_, &RF_prop, (RF_RadioSetup *)&RF_cmdPropRadioDivSetup, &rf_params);
if (!rf_handle_) {
CONSOLE_ERROR("SubGHzRadio::Init", "Failed to open RF device.");
return false; // Failed to open RF handle.
}

RF_EventMask ret = RF_runCmd(rf_handle_, (RF_Op *)&RF_cmdFs, RF_PriorityNormal, nullptr, 0);
if (ret != RF_EventLastCmdDone) {
CONSOLE_ERROR("SubGHzRadio::Init", "Failed to set frequency.");
RF_close(rf_handle_);
return false; // Failed to run command FS.
}

return StartPacketRx();
}

bool SubGHzRadio::DeInit() {
RF_close(rf_handle_);
return true;
}

bool SubGHzRadio::HandlePacketRx(rfc_dataEntryPartial_t *filled_entry) {
pico_ll.BlinkSubGLED();

/* Handle the packet data, located at &currentDataEntry->data:
* - Length is the first two bytes with the current configuration
* - Data starts from the second byte */
// rfc_dataEntryPartial_t *filled_entry = (rfc_dataEntryPartial_t *)rx_data_queue.pLastEntry;
uint8_t *buf = (uint8_t *)(&filled_entry->rxData);
uint16_t rxdata_bytes_after_len =
buf[0] | (buf[1] << 8); // 2-Byte length is packaged LSB first (little endian). Includes appended bytes.
uint16_t packet_len_bytes = rxdata_bytes_after_len - kPartialDataEntryNumAppendedBytes - kPacketHeaderSizeBytes;
// Note that filled_entry->nextIndex should == packet_len_bytes + kPartialDataEntryNumAppendedBytes.
uint8_t packet_sync_ls4 = buf[2] & 0x0F; // Last 4 bits of sync word are the first 4 bits of the payload.

if (packet_len_bytes > kRxPacketMaxLenBytes || packet_len_bytes == 0) {
return false;
}
uint8_t *packet_data = buf + kPartialDataEntryPayloadLenSzBytes + kPacketHeaderSizeBytes;

// Appended Bytes (no CRC)
//------------------------------------------
// | RSSI | TS0 | TS1 | TS2 | TS3 | Status |
//------------------------------------------

RawUATADSBPacket raw_packet = RawUATADSBPacket(packet_data, packet_len_bytes);
raw_packet.sigs_dbm = static_cast<int8_t>(packet_data[packet_len_bytes]);
uint32_t timestamp = packet_data[packet_len_bytes + 1] | (packet_data[packet_len_bytes + 2] << 8) |
(packet_data[packet_len_bytes + 3] << 16) | (packet_data[packet_len_bytes + 4] << 24);
raw_packet.mlat_48mhz_64bit_counts = timestamp;
int8_t status = static_cast<int8_t>(packet_data[packet_len_bytes + kPartialDataEntryNumAppendedBytes - 1]);
static_assert(kPartialDataEntryNumAppendedBytes == 6); // This section is hardcoded to match the appended bytes.
uat_packet_decoder.raw_uat_adsb_packet_queue.Enqueue(raw_packet);

return true;
}

bool SubGHzRadio::StartPacketRx() {
last_rx_start_timestamp_ms_ = get_time_since_boot_ms();
rx_cmd_handle_ =
RF_postCmd(rf_handle_, (RF_Op *)&RF_cmdPropRxAdv, RF_PriorityNormal, rf_cmd_callback, kRxEventMask);
if (rx_cmd_handle_ < 0) {
CONSOLE_ERROR("SubGHzRadio::Init", "Failed to post command PROP_RX: returned code %d.", rx_cmd_handle_);
return false; // Failed to post command PROP_RX.
}
return true;
}

bool SubGHzRadio::Update() {
volatile uint16_t rx_status = ((volatile RF_Op *)&RF_cmdPropRxAdv)->status;
if ((rx_status & 0xFF00) & PROP_DONE_OK) {
StartPacketRx();
} else if ((rx_status & 0xFF00) & PROP_ERROR_PAR) {
char *error_str;
switch (rx_status) {
case PROP_ERROR_PAR:
error_str = (char *)"Illegal parameter";
break;
case PROP_ERROR_RXBUF:
error_str = (char *)"No available Rx buffer at the start of a packet";
break;
case PROP_ERROR_RXFULL:
error_str = (char *)"Out of Rx buffer during reception in a partial read buffer";
break;
case PROP_ERROR_NO_SETUP:
error_str = (char *)"Radio was not set up in proprietary mode";
break;
case PROP_ERROR_NO_FS:
error_str = (char *)"Synth was not programmed when running Rx or Tx";
break;
case PROP_ERROR_RXOVF:
error_str = (char *)"Rx overflow observed during operation";
break;
case PROP_ERROR_TXUNF:
error_str = (char *)"Tx underflow observed during operation";
break;
default:
error_str = (char *)"Unknown error";
}
CONSOLE_ERROR("SubGHzRadio::Update", "PROP_RX threw error (0x%x): %s. Restarting.", rx_status, error_str);
StartPacketRx();
}

return true;
}
```
  • Hello John,

    I hope you are doing well. Have you tried wrapping the rf receive in a semaphore to prevent it from being interrupted? 

    Assuming that the rf data is more important prevent anything from interrupting the rf receive, as this could mess up the radio state and cause various issues. 

    Assuming that the SPI data is more important, cancel the ongoing receive as soon as possible (so the radio goes into a safe known state), send the SPI, and go back to receiving (*but miss packets in this case).

    Thanks,
    Alex F

  • Hi Alex,

    Thanks for the fast reply! I'm currently running this under the TI-NoRTOS kernel. Would I still be able to use a semaphore there? Could you provide an example code snippet to illustrate what you mean by using a semaphore for this?

    In this application the RF data is more important. We would want an rx callback interrupt to pre-empt any ongoing SPI callback interrupt (the SPI transaction can be delayed by up to 1ms without issue). The SPI peripheral is relatively slow and can send some large packets, so it would be nice if the receiver wasn't completely blind during an ongoing SPI transactiokn. Is there a way to accomplish this with interrupt priority changes only?

  • Hi Alex,

    Thanks for the fast reply! I'm currently running this under the TI-NoRTOS kernel. Would I still be able to use a semaphore there? Could you provide an example code snippet to illustrate what you mean by using a semaphore for this?

    In this application the RF data is more important. We would want an rx callback interrupt to pre-empt any ongoing SPI callback interrupt (the SPI transaction can be delayed by up to 1ms without issue). The SPI peripheral is relatively slow and can send some large packets, so it would be nice if the receiver wasn't completely blind during an ongoing SPI transactiokn. Is there a way to accomplish this with interrupt priority changes only?

  • Hello John,

    We can use the Semaphore by following something like this (and referencing the semaphore.c/.h file in the sdk):

     if (Semaphore_pend(dataSem, timeout)) {
            /* get message from dataQue */
            elem = Queue_get(dataQue);

            /* copy message to user supplied pointer */
            /* SV.BANNED.REQUIRED.COPY */
            (void)memcpy(msg, elem + 1, obj->msgSize);

            /* perform the enqueue and increment numFreeMsgs atomically */
            key = Hwi_disable();

            /* put message on freeQue */
            Queue_enqueue(freeQue, &(elem->elem));

            /* increment numFreeMsgs */
            obj->numFreeMsgs++;

            /* re-enable ints */
            Hwi_restore(key);

            /* post the semaphore */
            Semaphore_post(freeSem);

            return (true);
        }
        else {
            return (false);
        }
    Thanks,
    Alex F
  • Hi Alex,

    My understanding is that the semaphore is only available within TI-RTOS. Do you have a solution for this in the TI-NoRTOS kernel? I would have assumed that there would be a way to use interrupt priorities within the NVIC to make this work instead of using semaphores.

    John

  • Hello John,

    I apologize; my recommendation relies on semaphores which can't be used in NORTOS here. We could possibly use a hardware interrupt, or follow what the following code does (which disables hardware interrupts temporarily):

        /* Enter critical section */
        uint32_t key = HwiP_disable();
    
        /* Local variables */
        List_Elem* pTail = NULL;
        List_Elem* pHead = List_head(list);
    
        /* Start at the head of queue */
        while (pHead)
        {
            if (RF_isClientOwner(h, (RF_Cmd*)pHead))
            {
                pTail = pHead;
            }
    
            pHead = List_next(pHead);
        }
    
        /* Exit critical section */
        HwiP_restore(key);

    Thanks,
    Alex F

  • Hi Alex,

    I think the most promising solution I've found so far is to set maxPktLen on the rx command to the maximum packet size. I am still doing a partial rx and then attempting to end the transmission early by running the packet length set command as soon as I know how long the packet is. Do you know if this will still interrupt the receiving, even when maxPktLen is not set to 0 (unlimited length mode)? I've noticed that the packets produced by the RF core are still set to the maximum length defined by maxPktLen but haven't looked under the hood to see whether they are fully filled out yet.
    Setting maxPktLen stops the crashes I'm seeing, since even when the MCU is blinded by a SPI interrupt we don't end up writing infinitely into memory. The downside is that if the receiver is receiving the full maxPktLen every time despite being told a new length sometime after the start of the packet, we waste a lot of receive time ingesting bytes that were never transmitted.
  • Hello John,

    Here we could try keeping maxPktLen then adding RF_cancelCmd to the callback and execute if we figure out that the partial packet is not what we need and we don't need to read the rest of the packet; this way we can use a working configuration but end the transmission early if needed. 

    Thanks,
    Alex F

  • If I send RF_cancelCmd, will I still get RSSI / timestamp / etc for the packet?

  • Hello John,

    Assuming that the timestamp/etc packet information was received by the partial packet receive you should be able to use it; if we cancel the packet after the sync word is found then in that case we could lose the packet.

    Thanks,
    Alex F

  • I see, so RSSI and timestamp are filled out before the packet is complete? Or are they filled out even after a cancelCmd?

  • Hello John,

    To my knowledge the RSSI and timestamp are taken not by the info inside the packet but rather by the packet "detection" by the receiving device, by that I mean if the packet's preamble/sync word is accepted and we are in the process of receiving the packet we will have the RSSI and timestamp info be updated. 

    Thanks,
    Alex F