Part Number: CC1311R3
Tool/software:
Hi,
Using simplelink_cc13xx_26xx SDK 7.10.01.24
I use TI-RTOS and UART2 in blocking receiving mode with
I do not know the number of bytes to receive, but the first byte is the "uart length byte"
I call the UART2_read with size = 1 first.
I then expected the function to return after one byte.
However, it I get 6 bytes on UART then it waits until I have received all 6 bytes + hardware read timeout.(The hardware read timeout is not very well documented.)
Is it correct to assume that the UART2_read call should return immediately after I get one character in for my case?
-no-more-wires