This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BEAGL-PLAY-SBC: New build of TI Wi-SUN FANTund failed to compile

Part Number: BEAGL-PLAY-SBC


Tool/software:

Dear TI Engineers and Experts,

Today, I tried to build a new wi-sun border router on BeaglePlay board.

I did it many times so it should be an easy job.  However, it turned out failing at one step.

Here are my steps:

  1. Install Wi-SUN compatible BeaglePlay Debian OS 11.8 minimal image file from here:
    https://forum.beagleboard.org/t/arm64-debian-11-x-bullseye-monthly-snapshots-2023-10-07/32318

    beagleplay-emmc-flasher-debian-11.8-minimal-arm64-2023-10-07-4gb.img.xz


  2. everything goes well until here:

    cd /usr/local/ti-wisunfantund/ti-wisun-webapp/client/

    sudo npm install

    sudo npm audit fix                  (reducing the number of vulnerabilities; optional)

    sudo npm run build

    > utdesign-ti-wisunfan-webserver-client@1.0.0 build
    > react-scripts build
    
    Creating an optimized production build...
    Failed to compile.
    
    /usr/local/ti-wisunfantund/ti-wisun-webapp/client/src/components/Topology.tsx
    TypeScript error in /usr/local/ti-wisunfantund/ti-wisun-webapp/client/src/components/Topology.tsx(39,25):
    Namespace 'cytoscape' has no exported member 'Stylesheet'.  TS2694
    
        37 |
        38 | interface TopologyTheme {
      > 39 |   stylesheet: cytoscape.Stylesheet[];
           |                         ^
        40 | }
        41 | const topologyThemeImplementations = new ComponentThemeImplementations<TopologyTheme>();
        42 | const tiTopologyTheme: TopologyTheme = {
        



Please correct it as soon as possible!  Sob

  • Yes, I did it successfully many times, close to 50 successful builds

    Install Node.js v16.13.2
    ==================

    sudo apt install npm

    To install specific versions of Node.js n globally, run:
    sudo npm install -g n
    sudo n 16.13.2

  • Hi Tim,

    Do you mean you've done it before with a previous release of ti-wisunfantund but it fails with the current one?

    Best regards,

    Daniel

  • Hello,

    I renew ti wisunfand for every new installation as:

    cd /usr/local/
    sudo git clone github.com/.../ti-wisunfantund.git
    cd ti-wisunfantund

  • Hi Tim,

    I understand. I'll give this a test and come back to you.

    Best regards,

    Daniel

  • Hi Tim,

    I've started from a fresh installation using the BeaglePlay Debian OS 11.8 minimal image you linked to, the latest ti-wisunfantund and followed all instructions to the letter from INSTALL.md and README.md. Purposely I left out "sudo npm audit fix" and it works

    Here is the log:

    dBeaglePlay:/usr/local/ti-wisunfantund/ti-wisun-webapp/client$ sudo npm ru
    
    > utdesign-ti-wisunfan-webserver-client@1.0.0 build
    > react-scripts build
    
    Creating an optimized production build...
    Browserslist: caniuse-lite is outdated. Please run:
      npx browserslist@latest --update-db
      Why you should do it regularly: https://github.com/browserslist/browserslist#browsers-data-updating
    =============
    
    WARNING: You are currently running a version of TypeScript which is not officially supported by @typescript-eslint/typescript-estree.
    
    You may find that it works just fine, or you may not.
    
    SUPPORTED TYPESCRIPT VERSIONS: >=3.3.1 <4.5.0
    
    YOUR TYPESCRIPT VERSION: 4.5.5
    
    Please only submit bug reports when using the officially supported version.
    
    =============
    
    Compiled with warnings.
    
    src/APIService.tsx
      Line 2:9:  'Pingburst' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/App.tsx
      Line 5:8:  'ThemeToggle' is defined but never used     @typescript-eslint/no-unused-vars
      Line 7:9:  'PingJobsButton' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/BorderRouterConfigProperties.tsx
      Line 1:9:  'APIService' is defined but never used  @typescript-eslint/no-unused-vars
      Line 2:9:  'App' is defined but never used         @typescript-eslint/no-unused-vars
    
    src/components/BorderRouterInfoProperties.tsx
      Line 42:10:  'mainTextColor' is assigned a value but never used  @typescript-eslint/no-unused-vars
    
    src/components/ConfigPropertyInput.tsx
      Line 1:21:  'useRef' is defined but never used                            @typescript-eslint/no-unused-vars
      Line 3:9:   'NETWORK_TIMEOUT_WARNING_DURATION' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/ConfigPropertySelect.tsx
      Line 1:21:  'useRef' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/ConfigTab.tsx
      Line 3:9:   'ThemedInput' is defined but never used          @typescript-eslint/no-unused-vars
      Line 4:8:   'ThemedLabel' is defined but never used          @typescript-eslint/no-unused-vars
      Line 5:9:   'AppContext' is defined but never used           @typescript-eslint/no-unused-vars
      Line 6:8:   'produce' is defined but never used              @typescript-eslint/no-unused-vars
      Line 7:9:   'NCPNumberProperties' is defined but never used  @typescript-eslint/no-unused-vars
      Line 7:45:  'NCPStringProperties' is defined but never used  @typescript-eslint/no-unused-vars
      Line 12:9:  'useContext' is defined but never used           @typescript-eslint/no-unused-vars
    
    src/components/HealthMonitor.tsx
      Line 4:9:  'getIPAddressInfoByIP' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/InfoTooltip.tsx
      Line 141:6:   React Hook useLayoutEffect has a missing dependency: 'overflowCallback'. Either include it or remove the dependency array. If 'overflowCallback' changes too often, find the parent component that defines it and wrap that definition in useCallback  react-hooks/exhaustive-deps
      Line 358:17:  'InfoMessageTooltipCard' is already defined                                                                                                                                                                                                            @typescript-eslint/no-redeclare
      Line 397:17:  'InfoPropertyTooltipCard' is already defined                                                                                                                                                                                                           @typescript-eslint/no-redeclare
      Line 449:17:  'ErrorPropertyTooltipCard' is already defined                                                                                                                                                                                                          @typescript-eslint/no-redeclare
    
    src/components/LEDConfig.tsx
      Line 1:9:  'pointer' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/LEDObject.tsx
      Line 13:19:  Expected '===' and instead saw '=='  eqeqeq
      Line 16:26:  Expected '===' and instead saw '=='  eqeqeq
    
    src/components/LoadingTextBox.tsx
      Line 2:9:  'Color' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/MacFilterSettings.tsx
      Line 1:8:   'produce' is defined but never used                                                                       @typescript-eslint/no-unused-vars
      Line 80:5:  React Hook useCallback has a missing dependency: 'App'. Either include it or remove the dependency array  react-hooks/exhaustive-deps
    
    src/components/MonitorTab.tsx
      Line 1:8:     'Pane' is defined but never used          @typescript-eslint/no-unused-vars
      Line 4:8:     'AtAGlance' is defined but never used     @typescript-eslint/no-unused-vars
      Line 10:9:    'ColorScheme' is defined but never used   @typescript-eslint/no-unused-vars
      Line 10:22:   'THEME' is defined but never used         @typescript-eslint/no-unused-vars
      Line 10:29:   'ThemeContext' is defined but never used  @typescript-eslint/no-unused-vars
      Line 14:16:   'useContext' is defined but never used    @typescript-eslint/no-unused-vars
      Line 14:46:   'useEffect' is defined but never used     @typescript-eslint/no-unused-vars
      Line 16:10:   'gray' is defined but never used          @typescript-eslint/no-unused-vars
      Line 16:16:   'timer' is defined but never used         @typescript-eslint/no-unused-vars
      Line 17:10:   'stat' is defined but never used          @typescript-eslint/no-unused-vars
      Line 18:10:   'noop' is defined but never used          @typescript-eslint/no-unused-vars
      Line 19:10:   'current' is defined but never used       @typescript-eslint/no-unused-vars
      Line 58:68:   Expected '===' and instead saw '=='       eqeqeq
      Line 62:41:   Expected '===' and instead saw '=='       eqeqeq
      Line 74:38:   Expected '===' and instead saw '=='       eqeqeq
      Line 77:43:   Expected '===' and instead saw '=='       eqeqeq
      Line 80:43:   Expected '===' and instead saw '=='       eqeqeq
      Line 83:43:   Expected '===' and instead saw '=='       eqeqeq
      Line 86:43:   Expected '===' and instead saw '=='       eqeqeq
      Line 92:43:   Expected '===' and instead saw '=='       eqeqeq
      Line 103:32:  Expected '===' and instead saw '=='       eqeqeq
      Line 110:25:  Expected '===' and instead saw '=='       eqeqeq
      Line 111:32:  Expected '!==' and instead saw '!='       eqeqeq
      Line 114:31:  Expected '!==' and instead saw '!='       eqeqeq
      Line 117:31:  Expected '!==' and instead saw '!='       eqeqeq
      Line 120:33:  Expected '!==' and instead saw '!='       eqeqeq
    
    src/components/NCPStatus.tsx
      Line 21:12:  'wasSuccess' is assigned a value but never used  @typescript-eslint/no-unused-vars
    
    src/components/NetworkProperties.tsx
      Line 1:34:  'useEffect' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/OADInterface.tsx
      Line 1:9:     'pointer' is defined but never used                   @typescript-eslint/no-unused-vars
      Line 2:28:    'useReducer' is defined but never used                @typescript-eslint/no-unused-vars
      Line 5:9:     'CytoscapeGraph' is defined but never used            @typescript-eslint/no-unused-vars
      Line 6:8:     'LEDObject' is defined but never used                 @typescript-eslint/no-unused-vars
      Line 9:8:     'cytoscape' is defined but never used                 @typescript-eslint/no-unused-vars
      Line 10:8:    'CytoscapeComponent' is defined but never used        @typescript-eslint/no-unused-vars
      Line 11:10:   'useForceUpdate' is defined but never used            @typescript-eslint/no-unused-vars
      Line 12:10:   'PassThrough' is defined but never used               @typescript-eslint/no-unused-vars
      Line 13:10:   'ErrorPropertyTooltipCard' is defined but never used  @typescript-eslint/no-unused-vars
      Line 14:10:   'readFileSync' is defined but never used              @typescript-eslint/no-unused-vars
      Line 35:10:   'fileData' is assigned a value but never used         @typescript-eslint/no-unused-vars
      Line 35:20:   'setFileData' is assigned a value but never used      @typescript-eslint/no-unused-vars
      Line 84:30:   Expected '===' and instead saw '=='                   eqeqeq
      Line 89:17:   Expected '===' and instead saw '=='                   eqeqeq
      Line 116:28:  Expected '===' and instead saw '=='                   eqeqeq
      Line 129:30:  Expected '===' and instead saw '=='                   eqeqeq
    
    src/components/PaneContainer.tsx
      Line 2:20:  'useContext' is defined but never used                     @typescript-eslint/no-unused-vars
      Line 3:9:   'ColorScheme' is defined but never used                    @typescript-eslint/no-unused-vars
      Line 3:22:  'THEME' is defined but never used                          @typescript-eslint/no-unused-vars
      Line 3:29:  'ThemeContext' is defined but never used                   @typescript-eslint/no-unused-vars
      Line 5:9:   'ComponentThemeImplementations' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/PingConfig.tsx
      Line 13:8:    'Tooltip' is defined but never used                  @typescript-eslint/no-unused-vars
      Line 16:3:    'InfoPropertyTooltipCard' is defined but never used  @typescript-eslint/no-unused-vars
      Line 143:31:  Expected '===' and instead saw '=='                  eqeqeq
    
    src/components/PingJobMonitor.tsx
      Line 5:9:   'getIPAddressInfoByIP' is defined but never used     @typescript-eslint/no-unused-vars
      Line 7:52:  'NumberOfPacketsQuantity' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/PingLog.tsx
      Line 3:9:   'getIPAddressInfoByIP' is defined but never used   @typescript-eslint/no-unused-vars
      Line 5:9:   'sort' is defined but never used                   @typescript-eslint/no-unused-vars
      Line 6:53:  'timestampStringToDate' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/SuccessRateLineChart.tsx
      Line 5:24:  'Pingburst' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/Tooltip.tsx
      Line 1:27:  'RefObject' is defined but never used  @typescript-eslint/no-unused-vars
      Line 1:38:  'useEffect' is defined but never used  @typescript-eslint/no-unused-vars
    
    src/components/Topology.tsx
      Line 1:16:    'useContext' is defined but never used            @typescript-eslint/no-unused-vars
      Line 1:28:    'useState' is defined but never used              @typescript-eslint/no-unused-vars
      Line 6:8:     'produce' is defined but never used               @typescript-eslint/no-unused-vars
      Line 9:33:    'InfoTooltip' is defined but never used           @typescript-eslint/no-unused-vars
      Line 9:46:    'InfoTooltipMode' is defined but never used       @typescript-eslint/no-unused-vars
      Line 210:14:  'stylesheet' is assigned a value but never used   @typescript-eslint/no-unused-vars
      Line 242:7:   'OADFWString' is assigned a value but never used  @typescript-eslint/no-unused-vars
    
    src/hooks/useForceUpdate.ts
      Line 4:10:  'value' is assigned a value but never used  @typescript-eslint/no-unused-vars
    
    src/hooks/useLoc.ts
      Line 1:20:  'useEffect' is defined but never used                                                                                                        @typescript-eslint/no-unused-vars
      Line 32:6:  React Hook useLayoutEffect has missing dependencies: 'bottom', 'right', and 'targetRef'. Either include them or remove the dependency array  react-hooks/exhaustive-deps
    
    src/types.tsx
      Line 3:10:  'StringLiteral' is defined but never used  @typescript-eslint/no-unused-vars
    
    Search for the keywords to learn more about each warning.
    To ignore, add // eslint-disable-next-line to the line before.
    
    File sizes after gzip:
    
      358.46 KB  build/static/js/2.6ca26b43.chunk.js
      38.52 KB   build/static/js/main.68701475.chunk.js
      1.96 KB    build/static/css/main.2a90219b.chunk.css
      797 B      build/static/js/runtime-main.79fab79a.js
    
    The project was built assuming it is hosted at ./.
    You can control this with the homepage field in your package.json.
    
    The build folder is ready to be deployed.
    
    Find out more about deployment here:
    
      https://cra.link/deployment
    
    debian@BeaglePlay:/usr/local/ti-wisunfantund/ti-wisun-webapp/client$

    I deleted the build/ directory, ran sudo npm audit fix  and tried to build it again. This time I get the same error as you.

    n buildBeaglePlay:/usr/local/ti-wisunfantund/ti-wisun-webapp/client$ sudo npm ru
    
    > utdesign-ti-wisunfan-webserver-client@1.0.0 build
    > react-scripts build
    
    Creating an optimized production build...
    Failed to compile.
    
    /usr/local/ti-wisunfantund/ti-wisun-webapp/client/src/components/Topology.tsx
    TypeScript error in /usr/local/ti-wisunfantund/ti-wisun-webapp/client/src/components/Topology.tsx(39,25):
    Namespace 'cytoscape' has no exported member 'Stylesheet'.  TS2694
    
        37 |
        38 | interface TopologyTheme {
      > 39 |   stylesheet: cytoscape.Stylesheet[];
           |                         ^
        40 | }
        41 | const topologyThemeImplementations = new ComponentThemeImplementations<TopologyTheme>();
        42 | const tiTopologyTheme: TopologyTheme = {

    There is clearly an issue with dependencies. I took a dump of the "audit fix --json" I will share with the developers. But I suggest you build it without running npm audit fix.

    Best regards,

    Daniel

  • Yeah!  Let me try!  Thanks! Laughing