Other Parts Discussed in Thread: CC1200
Hello, I am using the SRFS 7 (v. 2.32.0 ) offline on a Win10 platform to setup the registers configuration of a cc1200 device, and then to export it to my code...
The problem is that if I use the 'Save Cfg' menu command in the tool, it appears I can save my last edited configuration, but if want to resume it later, with the 'Open Cfg' menu command and load the last saved Cfg, the configuration loaded seems missing most of the parameters, or they appear to be even different from the ones I saved... For example the Symbol Rate is always set to 1.2 ksps, of Modulation to 2-FSK while I saved 9.6Ksps in 2-GFSK mode, sometimes it looses the Range extender ( CC1190EM ) settings, sometimes not...Even some registers in the Register View appears to be set to randomic values...
This would eventually make RED certifications problem fixings impossible using this tool, because, if I want to change even single settings in the registers using this tool, I can not be sure of the result and that no other 'unwanted' registers have been affected...
Any fix to this...?
Am I the only one having this problem...?
Thanks for any support...
Kind Regards
Alex