Part Number: CC1310
We are considering evaluating the 718–878 MHz band using the LAUNCHXL-CC1310. According to the CC1310 datasheet, it is stated that this frequency range can be used if the necessary parameters are provided. If we receive the data, can we immediately start evaluation with the LAUNCHXL-CC1310?