This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: ROM Bootloader

Part Number: CC1310

Hi Team,

Posting on behalf of our customer.

I designed a custom PCB based on the CC1310 reference design. In my board, I did not route the JTAG programming interface, because I intended to program the device through the UART ROM bootloader.

I am using the CC1310 in the 7×7 package and connected the UART bootloader pins through DIO2 and DIO3. I power the board with 3.3 V and try to communicate with the device using a Python script over UART, but I do not receive any response from the chip.

At the moment, the board does not acknowledge any bootloader communication attempt, and the result is effectively “No Response.”

Could you please advise what conditions are required for the CC1310 to respond through the UART bootloader on a fresh board, and what hardware or boot configuration points I should verify?

I would also appreciate your help confirming whether the issue could be related to:

- Bootloader entry conditions
- Reset or power sequencing
- UART pin usage on DIO2/DIO3
- Any required hardware connections that may have been missed in the design

Regards,

Danilo