in the swrc117
is funny,the cc11xx-cc25xx are mainly RF chips,where their RF features are the main thing,and you can see on the swrc117 examples,there is only one RF example ,sending nothing,handling nothing...even the most nice features like hopping protocols,manual,and automatic packets,some elemental rF macros and fuctions are also missing,(the old cc1010 is well documented on RF macros and fuctions and it was back in 2004)
where I can download more RF examples for the cc11xx-cc25xx Soc?? dont send me the swrc021f because of the keil and the c8051 and the pins and the hole thing are a bit different