Hi All,
I am very new to SimpliciTI and need some help. Appreciate if someone can advice me on the following:
1) Set Pin 3 (P2.0/ACLK/A0/OA010) on the eZ430-RF2500 to output (Pin 3 is connected to +ve leg of LED. The -ve leg is connected to ground)
2) Set Pin 3 to high to light up the LED for 100 microsecond (need to activate the 16 bit timer counter - 0.0625 microsecond resolution)
3) Set Pin 3 to low for 10 millisecond (continues looping 2 and 3)
Thanks.
Irwan