This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2511 USB/DMA/SimpliciTI flow control

Other Parts Discussed in Thread: SIMPLICITI

Has anyone modified the USB framework code used in the RF USB Libraries (rs232_to_usb example) and examples to use DMA instead of polling? My application receives RF packets (@250Kbps, 16 byte app payload) from SimpliciTI but isn't fast enough to guarantee that the packet payload will be written  to the USB IN (EP4) without occassional data loss. Do you think using dma on the USB fifo would would speed things up? Does simpliciTI  protocol have any built in flow control i.e. if rx queue is  full, will the sending peer be told to wait and if so, is this flow control hidden from the sending app or must the app detect that the Smpl_send has failed and reattempt?

JW