I'm trying to use the demo code for SimpliciTI on CC2430DK platform. I create the project for a peer to peer connection in keil uVision3, and also create and add required config files.
The code is compiled and DKs start up, but wanna connect to each other they do not work properly. Debugging the program I understand the chip dose not detect any data even an SFD.
what should I do?