This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2430 HAL code library?

Other Parts Discussed in Thread: Z-STACK, CC2430, CC2510

Is there a complete set of HAL code for the CC2430?  I have a development kit, and basically just want a relatively simple hardware abstraction code set upon which to build myapplications.  I have seen that that Z-stack does include alot of HAL code, but I find it quite awkward to use particularly when implementation of Zigbee is not my intention for the CC2430.  I noticed that the software examples (SWRC019) have a nice set of HAL code but it is incomplete (UART is not implemented for example).

Thanks,

Alex.