Hi,
I have a problem with Z-Tool. I'm working with ZigBee-Stack 2.1.0-1.3.0 and Z-Tool 2.0. I send some debugging messages to Z-Tool and besides the information in the message I also need the timestamp. Everything works fine expect the timestamp itself. Here are some example timestamps I obtain from Z-Tool:
19:36.069
19:36.708
19:36.631
It seems that the seconds are missing. 19:36 are the hours and the minutes and 069, 708, 631 seem to be the milliseconds. Is there a way to change the displayed format or do I have a wrong understanding of the format? Or is it possible that this is a bug of Z-Tool 2.0 for ZigBee-Stack 2.1.0-1.3.0?
Thank you very much.
Regards,
Pascal