Hi,
first of all - I have not used Simpliciti yet, just read several documents and sources and some questions arise:
It seems that typically one - always on - AP is required. How much power is required for this AP? What is his state most of the time? (my guess: receiver?). Is it possible to tell the AP (and all endpoints) that the AP is sleeping for the next e.g. 100ms and the endpoints transmit only when the AP is awoken?
What I want is a simple point-to-point connection with both tranceivers sleeping most of the time (both are battery powered). After both points have been synchronized they switch the tranceiver for e.g. 100ms in sleep mode and wake up in fixed 100ms intervals to transfer some bytes and keep the sync. It should be possible to enlarge this period to one second or one minute ormuch longer. Is this possible with SimpliciTi?
In the approach above: I want to change the channels regularly on both sides (because of the crowed 2.4GHz band) eg: after 100ms: ch1, after 200ms: ch17 ,300ms ch:8 ... If there is noise at ch17 or no response, the same block will be retransmitted at ch 8 in the next interval (and so on until there is a free channel or a response). The channel tables are fixed and well known for both points. Does SimpliciTi support this simple frequency hopping scheme?
Thx Leo