Hi, Guys! I’m a college student who’s learning SimpliciTI, and trying to develop some applications on it. I compile and download the “AP as data hub” project on IAR 51 V7.40B, using the CC1110 Module. Everything goes on well when I only use AP and EDs. However, when I try to add a RE in the network, trouble comes.
1. The “SimpliciTI Range Extender - Release” is in the project, but I couldn’t download it to the board at all. I enter the Options for “SimpliciTI Range Extender”, and find out that the whole page (all the options) in DebuggeràTexas Instruments is disabled!
When I click the Debug button, the process bar shows up and disappears within half a second, and the code actually hasn’t been download at all.
Is there any option I should change to download the RE code?
2. When I start a new project to include all the files in the “SimpliciTI Range Extender” of the project “AP as data hub”, I can download it successfully. But it seems that the RE doesn’t work at all. Is it because I didn’t configure the network correctly, or because the RE couldn’t be used directly? I've already set the nodes with different addresses.
Hope you guys could help me out. Thanks!