Hi,
I am still confused with some definitions, so maybe someone can kindly explain.
According to http://en.wikipedia.org/wiki/6LoWPAN :
"The 6lowpan group has defined encapsulation and header compression mechanisms that allow IPv6 packets to be sent to and received from over IEEE 802.15.4 based networks"
Although 6LoWPAN can use a different physical layer (power lines, ...) is the radio layer restricted to 802.15.4 standard?
Some of TI's transceivers (like CC1101, CC430F..., CC1180) are not 802.15.4 compatible, yet they are listed as 6LoWPAN devices.
Where would I find a proper definition for 6LoWPAN?
As CC1101 is programmable, can it be made compatible with 802.15.4 and if not why?
Can I make the CC1180 (Sensinode stack) talking to CC1101 running Contiki (as both are running IPv6 and have the same physical layer)?
Regards
Jan