This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

My Range Extender doesn't increase the range of my network

Other Parts Discussed in Thread: SIMPLICITI

Hello,

I'm trying to implement a network by using the EZ430RF  Polling_With_AP Application of Simpliciti.I want it to be an ED-AP-RE-ED.

The goal of the Range Extender is, of course, to extend the range of the network. Unfortunately, it doesn't work :

I made "range tests" in a building with a "Sender-AP-Receiver". The maximum range between the Access Point and an ED was about 40m, after that, it doesn't receive any frames.

Then, I tried with "Sender-AP-Range Extender- Receiver", but the new range of the network is...the same (there was 20m between the AP and the RE). Why doesn't it work?

I made the tests this way : I turned on all the devices (which are on batteries) and i moved away with one ED until the sniffer doesn't find anything.

The sniffer indicates that the RE works properly (it repeates the frames well), but the range is not extended.

Do you have an idea to fix it?

Thanks