I Have..................
I have seven system lets say System1,System2,.............................,System7
and seven battery operated remote with 12 buttons lets say Remote1,Remote2,Remote3,Remote4.....Remote7
all of this have MCU and CC1101
I Want To Develop..................
Each system can send and receive data (1 byte or max 2 byte) from other systems
Each Remote can only send and receive data with corresponding System only . For ex :: remote1 to system1
and vice versa but remote1 to system2 must not be done
all of this systems are in 100 meters area
please reply is it possible or not if possible than where to start .............
THANKS