This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using CC2510 EM or CC2511 on SmartRF05 EB with SimpliciTI

Other Parts Discussed in Thread: CC2511, CC2510

1. The SmartRF05 EB comes with CC2533 EM and there are some software examples. Is there any example for CC2510 EM and CC2511  that assembled on the SmartRF05 EB? Maybe I need to change the SmartRF05 EB firmware or load dedicated examples (from where?).

2. How can I configure the MAC address or ID and Group address on the CC2510 EM and CC2511? I intend to use the SimpliciTI for CC2510 EM (or CC2511) that assembled on the SmartRF05 EB. Regarding the MAC address, I saw that it is included in the ZigBee protocol but not in the SimpliciTI. There is a dedicated address in the Flash for the MAC address or ID address.