Hi!
I want to make a simple link between Chronos 868(cc430f6137) and Anaren BoosterPack(CC110L).
To start i'm trying to send packets from Chronos to CC110L and vice versa. The problem is that sync word detection interrupt does not occur.
It's strange for me because CC110L to CC110L and Chronos to Chronos connections works properly, settings are the same and exported from SmartRF Studio 7.
Anyone can explain if there are any differences in register settings between cc430f6137 & CC110L radios that I could not consider?
It would be nice if someone shared example code of communication or at least settings of these radios.
I will be grateful for any help!
Alex