This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

4G LTE decreases the LPRF 868Mhz range with 2/3.

Other Parts Discussed in Thread: CC1190, CC1101, CC1120, CC1000

In Europe 4G networks based on LTE started to be implemented and they are using the 800MHz bands. Sweden and Germany already have installations and other countries are on their way to auction the bands.

Most LPRF applications in the EU is using the 868MHz band and external tests shows that the range is decreased with 2/3 or more. What are Texas recommendatios to the LPRF market, filters?, SW? Are there new Evaluation boards being developed that addresses the issue with coexistence with 4G?

When the 4G phones becomes the new standard phones many applications will suffer.