Hi
I have encountered a problem with SmartRF05EB(Ver1.8.1) that I have been using for 2 years. It was working well until yesterday. I have tried update the firmware. At first I may have put CC2530EM while updating the firmware. Then I disconnected EM and tried updating again. I didn't confirm well what firmware I wrote actually.
Finally the LED6 does not lit at all and PC does not recognize the USB. I tried everything in "SmartRF05 Evaluation Bord User's Guide" chap10 such as P18 pin17,19 short or using another board(alive) P2, P3 connect etc. But still LD6 does not lit. I believe the HW is OK.
If the U3(CC2511-F32) firmware corrupted, can I remove the device and put the new one(which is empty) and wrie the firmware? But I guess the Windows does not recognize the device.
Condition: Windows XP pro SP3, Flash Prorammer: ver1.12.5
Could anyone give me any advice?
Thanks.