Hi All,
one little question. Does the register CLKCONSTA only reflect the state of the clock settings or does it also show that a clock is stable? I am considering removing the 32kHz crystal and wonder whether this is possible without changes in the TI startup code that enables the crystal and polls for CLKCONSTA to be set. A quick test shows that it is possible to remove the crystal and get CLKCONSTA.OSC32K = 0.
Thanks in advance.
Best regards,
Tobias