This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem In communication Between CC1101 and CC430F6137 (EZ430-Chronos)

Other Parts Discussed in Thread: CC1101, CC430F6137

Hi 

When I used two CC1101 module then there is good communication between both module. But when I used one CC1101 as receiver and one CC430F6137 (EZ430-Chronos developement board) as transmitter, I am not getting anything in CC1101 module. But CC430F6137 is transmitting some data. I checked this using Spectrum Analyzer. I also keep the RF_Setting Configuration same in both module. Can someone please tell me what may be the possible cause. What precaution should be taken while communication one CC1101 and one CC430F6137 module.

Thanks 

Vivek