Hello I hope some one can help me on this problem of mine.
I am using a CC1110F32 chip on a development board (SmartRFCC1110-868) to build a system that communicates via wireless.
I managed to create a code to send and receive messages as I want I used pear to pear mode.
Now my question is about power management low power, power consumption, and in the system that I am developing the slave it powered by batteries.
My system needs to receive messages from a master when this sends them and it has to send messages from time to time and when a external interrupt is activated.
So in order to do this what power mode should I use? Can I put the device to sleep and make it wake up to attend a external and timer interrupt as well as a message from master is received?
Is it a good practice to hold the code with a while(1)? Or is there a better way to hold the device?
I hope that some one can answer me.