Hi ,
I'm using CC2500 and cc2511 transceivers in my project.One in transmitting data, and the other is receiving
I am using cc2500 at target board and cc2511 at host side.
I am able to communicate this two device at 2.5 Kbps.
My question is, how can I get the 500kbps and 250Kbps transmission rate??
I tried register value generate from smart RF studio for both cc2500 and cc2511 but some how i am not able to trans receive .my Xtal frequency for cc2500 is 2410MHz and for cc2511 is 48MHz.
I tried various setting like change in filter bandwidth ,deviation ,modulation format but badly i am not able to communicate this two chip at 250 and 500 Kbps.
please give me register setting or help to solve this problem.
Thanks in advance