This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC254x Timers and Clock Syncronization

Could a TI engineer shed some light on how the system clock is synchronized with the divided clock in the timer modules?  I have an application dictated necessity to synchronize the compare outputs on two different timers operating at different clock divisors.  Essentially, I need to run synchronized PWM on many output channels, and due to battery constraints, need to guarantee the outputs are mutually exclusive.

A little information about the clocking architecture could help me achieve this.  For example, are the different divisor clocks derived from a single clock divider, or are they independent per timer?  When does the divider start ticking relative to the system clock -- is an enable latched when the timer enable is first set, or is some other mechanism used?

If I set the enable bits for each timer in back to back assembly instructions, will that guarantee the timers are sync'd within 1-2 system clocks?  Or will the enable outputs be synchronized into the divided clock domain, and thus subject to a delay until the next divided clock tick?  In the later case is it possible to monitor the state of the divided clock, so that I may set enables when both clocks are in the desired start state?