Hello,
Sorry for asking again but didn't got answer there..
I'm working with TRXEB (rev 1.7) board, with cc1120 transceiver.
I've Downloaded the 1781.SimpliciTI-IAR-1.2.1-Beta file from this thread.
I've used the IAR to program the project Simple_peer_to_peer.
For some reason I can't get a working link:
I can see the LinkListen arriving to the linkFrom func' but never did he hears the LinkTo.. (so no link is established).
The linkTo never succeed in creating link, SMPL_Link func always fails.
This isn't a hardware issue, I've tested it with SMARTRF and all works OK (in both 900 & 800 MHz).
[as well as the example per test in the CC1120DK project]
What am I'm missing?